Skip to main content
Associate II
October 29, 2024
Question

Determine the component of "SB1" in STM32F407G-DISC1

  • October 29, 2024
  • 4 replies
  • 2190 views

Could someone help identify the part number and range for the SB1 component on the STM32F407G-DISC1 board? I'm interested in understanding its exact specifications.

4 replies

PGump.1
Senior II
October 29, 2024

Hi,

SB1 is a Solder Bridge. You can find the specifications from:

https://en.wikipedia.org/wiki/Solder 

I hope that helps.

Kind regards
Pedro

AI = Artificial Intelligence, NI = No Intelligence, RI = Real Intelligence.
Associate II
October 29, 2024

Is it necessary to keep solder bridge in custorm board ?

PGump.1
Senior II
October 29, 2024

Only you can decide that...

Kind regards
Pedro

AI = Artificial Intelligence, NI = No Intelligence, RI = Real Intelligence.
Andrew Neil
Super User
October 29, 2024

@rohithinthingstech wrote:

Could someone help identify the part number and range for the SB1 component on the STM32F407G-DISC1 board? I'm interested in understanding its exact specifications.


As already noted, "SB" is a Solder Bridge:

AndrewNeil_0-1730194887239.png

Just like a Jumper ("JP") it allows a connection to be easily made (closed) or broken (opened) - to allow configuration to a user's requirements.

https://electronics.stackexchange.com/questions/261106/solder-bridge-in-schematics-and-0-resistors

They use these Solder Bridges rather than traditional Jumper links because:

  • They are cheaper
  • They are smaller
  • They are easier for board assembly.

In some cases, rather than just use a "blob" of solder, a zero-ohm resistor (aka "zero-ohm link") will be fitted:

https://en.wikipedia.org/wiki/Zero-ohm_link

Here's an example - where SB53 (at the top) is "closed" with a zero-ohm link, and the others are "open":

AndrewNeil_2-1730198156522.png

 


Note that, in some cases, the pads of a Solder Bridge may have a track connecting them; eg,

AndrewNeil_2-1730195623906.png

https://www.reddit.com/r/KiCad/comments/p2bg9y/solder_jumper_usage_conceptual_question/

To "break" this kind of bridge, you need to cut that track.

I don't think that ST use this type - but other manufacturers certainly do

 

#SolderBridge #SB 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
AlexWEI
ST Employee
November 13, 2024

hi, you can refer the SBx as 0 ohm Res on board for cutting or connecting lines .