Skip to main content
Associate III
August 8, 2025
Question

Difference between F446RE & F446ZE Nucleo

  • August 8, 2025
  • 3 replies
  • 458 views

Hello... can anyone advise on the difference between F446RE and F446ZE? i just found out the USART to USB VCP was shifted to USART3 instead of USART2 in the new ZE. Can anyone advise on any other difference? 

3 replies

Andrew Neil
Super User
August 8, 2025

You could look at the two User Manuals:

 

F446RE: UM1724, STM32 Nucleo-64 boards (MB1136)
via: https://www.st.com/en/evaluation-tools/nucleo-f446re.html#documentation

F446ZE: UM1974, STM32 Nucleo-144 boards (MB1137)
via: https://www.st.com/en/evaluation-tools/nucleo-f446ze.html#documentation

 

Also the schematics - see the 'CAD Resources' tabs on those Product Pages.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Tesla DeLorean
Guru
August 8, 2025

Well apart from them being entirely different boards, with different pin counts, and escape to different headers, etc

Same IC / DIE, so 180 MHz, 512 KB Flash, 128 KB RAM

QSPI Escaped

Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..
Andrew Neil
Super User
August 8, 2025

@Tesla DeLorean wrote:

 entirely different boards, with different pin counts


Indeed:

AndrewNeil_2-1754669056435.png

 

 

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Tesla DeLorean
Guru
August 8, 2025

It's my view that you'd need to do a complete reappraisal of the pin usage, and look at all the stubs and escape paths to the different header arrangement.

It doesn't implement the Ethernet of the other NUCLEO-144's for parts that do, and I'd expect the Arduino shield connections to be going to different pins also.

One of the big issues with the NUCLEO-64 designs is that the Arduino shield D0/D1 clashed/share a UART resource with the VCP, and this gets avoided with more pins and UART escaped.

The double wide Arduino connector is a challenge, not seen a breakout / protoboard

You need different X-NUCLEO-GFX shields for NUCLEO-64 vs 144

https://www.st.com/en/evaluation-tools/x-nucleo-gfx01m1.html

https://www.st.com/en/evaluation-tools/x-nucleo-gfx01m2.html

https://www.st.com/en/evaluation-tools/x-nucleo-gfx02z1.html

 

Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..
Tesla DeLorean
Guru
August 8, 2025

>>I just found out the USART to USB VCP was shifted to USART3 instead of USART2

This is somewhat of a blessing, as now the F4 has a different UART for the Arduino D0/D1 pins from that of the VCP, so you can now use BOTH

Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..