It appears these Samtec connectors will mate to the ST DSI-to-HDMA connector but these are all board mount connectors that may require a custom circuit board as I can't find anything that will handle these.
Next question. Are there any ST boards that will plug directly to the DSI port on this adapter?
Thanks for the information. I'm not sure this particular adapter (B-LCDAD-HDMI1) is the interface I need to make this project work. I've started a related thread regarding the DSI interface and DSI LCD to gain more knowledge about how to use these displays.
I'm wading through these along with some other docs and code I've found. At this point I think I've chosen the wrong display for my purposes not to mention this DSI display has put me in way over my head for now. I was looking for something simple that apparently doesn't exist to make this work. Not really surprising considering access to the formal specs for the MIPI-DSI interface cost $2000+, as a member. There's also a number of docs and links from my other thread on the topic that I'll review, too.
Yes, well really just a low pin count way of funnelling data to the panel.
The DSIHOST serializes frame data spilling from the LTDC
The LTDC is just rendering lines from the frame buffer.
How the MCU interacts with the frame buffer is pretty much consistent, and same model for 40+ years
DSI is just a way of doing some of the plumbing, and usually not something you need to get deeply involved in, just have to get the bandwidth and timing ducks all lined up. DSI throughput needs to meet/exceed the delivery out of the LTDC.
Parallel RGB output is the most basic form, just eats a lot of pins, and isn't flexible as to which. Gets to be an exercise in board design and cabling.
You want to find panels with a design win in phones or tablets, and ride the wave of millions of units someone else is buying.
Also watch that life cycles for specific panels are apt to be 18-24 months, not 5-10 years.
Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..
It's funny you should say 'ride the wave'. It appears that most of these oddball sized LCD units available from places like Aliexpress are actually pulled from some sort of non-working (not the LCD) products, have an HDMI-DSI board attached then sold used. Looks like whatever product they take the LCDs from are products that we never see here.