ESD diode selection
Hi, I am designing a PCB using STM32G0B1RE to be deployed in automotive environment. I need to add ESD protection on its GPIO and ADC pins. I was going through AN5612: ESD protection of STM32 MCUs and MPUs. (Since any specific STM32 family is/are not mentioned in the doc, I think that it should be applicable to all the families.) Under subsection "3.3.4 Other serial interfaces", for I2C-bus ESD protection, the suggested part no. is USBLC6-4. Its electrical characteristics (see attached image) mentions that its V_BR (min) is 6.1V.

As per the STM32G0B1RE datasheet, the maximum allowable voltage on any pin is 4.0V to 5.5V (depending on the pin).

As per my understanding, V_BR of the ESD diode should be less than the AMR (Absolute Maximum Rating) of the concerned pin. My doubt is that whether the above mentioned ESD diode would be appropriate or are there some other parameters that are needed to be taken into consideration?
What is the best approach to select the ESD diodes for ADC and GPIO pins (max. 3.3 working voltage)?