Skip to main content
Associate III
September 29, 2025
Solved

GPIO , Button detection ( USER1) on STM32N6570-DK

  • September 29, 2025
  • 3 replies
  • 371 views

Post edited by ST moderator to be inline with the community rules especially with the code sharing. In next time please use </> button to paste your code. Please read this post: How to insert source code

Hi  , 

I’m currently playing around with the STM32N66570-DK kit.

I’m having a simple problem with button detection. For testing, I’m just using the USER1 button  (BP1 in my code ) and LED1.

I couldn’t get the button working properly with interrupts, so in this code I just read the state of USER1 ( BP1) and turn LED1 on or off accordingly.  The USER1 button is always read as the same value, no matter whether I press it or not.  

 

in debug Mode : 

GPIOx const GPIO_TypeDef * 0x56020800
GPIO_Pin uint16_t 8192
bitstatus GPIO_PinState GPIO_PIN_RESET

 

Here are the code and screenshots. The code was generated with CubeMX.

Thanks for your help!

Once I get the button detection working, I’ll move on to using interrupts.

Emmanuel

main.h :

#define BP1_Pin GPIO_PIN_13
#define BP1_GPIO_Port GPIOC
#define LED1_Pin GPIO_PIN_1
#define LED1_GPIO_Port GPIOO

 

main.c :

/* USER CODE BEGIN WHILE */

while (1)

{

/* USER CODE END WHILE */



/* USER CODE BEGIN 3 */

// code to test the LED1

//HAL_GPIO_WritePin(LED1_GPIO_Port, LED1_Pin, GPIO_PIN_SET);

//HAL_Delay(500);

//HAL_GPIO_TogglePin(LED1_GPIO_Port,LED1_Pin);



// Read the button USER1



if(HAL_GPIO_ReadPin (BP1_GPIO_Port, BP1_Pin) == GPIO_PIN_RESET)

{



//Turn LED ON

HAL_GPIO_WritePin(LED1_GPIO_Port, LED1_Pin, GPIO_PIN_SET);

}

else

{

//Turn LED OFF

HAL_GPIO_WritePin(LED1_GPIO_Port, LED1_Pin, GPIO_PIN_RESET);

}

}

/* USER CODE END 3 */

}



-----------------------------------------------------------



static void MX_GPIO_Init(void)

{

GPIO_InitTypeDef GPIO_InitStruct = {0};

/* USER CODE BEGIN MX_GPIO_Init_1 */

/* USER CODE END MX_GPIO_Init_1 */



/* GPIO Ports Clock Enable */

__HAL_RCC_GPIOC_CLK_ENABLE();

__HAL_RCC_GPIOO_CLK_ENABLE();



/*Configure GPIO pin Output Level */

HAL_GPIO_WritePin(LED1_GPIO_Port, LED1_Pin, GPIO_PIN_RESET);



/*Configure GPIO pin : BP1_Pin */

GPIO_InitStruct.Pin = BP1_Pin;

GPIO_InitStruct.Mode = GPIO_MODE_INPUT;

GPIO_InitStruct.Pull = GPIO_NOPULL;

HAL_GPIO_Init(BP1_GPIO_Port, &GPIO_InitStruct);



/*Configure GPIO pin : LED1_Pin */

GPIO_InitStruct.Pin = LED1_Pin;

GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;

GPIO_InitStruct.Pull = GPIO_NOPULL;

GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;

HAL_GPIO_Init(LED1_GPIO_Port, &GPIO_InitStruct);



/* USER CODE BEGIN MX_GPIO_Init_2 */

/* USER CODE END MX_GPIO_Init_2 */

}

 

Best answer by mfgkw

One more issue: following your code you have no pull up or pull down resistor to define the state of PC13 if the button is open.

Following the MB1939-N6570-C02 Board schematic (https://www.st.com/resource/en/schematic_pack/mb1939-n6570-c02-schematic.pdf) the button switches to 3v3. There is a resistor R225 (10k) to GND, but marked as DNF.

So I suggest to enable an internal pull down for the button GPIO to be sure.

3 replies

mƎALLEm
Technical Moderator
September 29, 2025

Hello,

You share a bed resolution images.

But to be sure, is MX_GPIO_Init() called in the main before the while loop. You shared only the while loop.

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question."
mfgkwBest answer
Associate II
September 30, 2025

One more issue: following your code you have no pull up or pull down resistor to define the state of PC13 if the button is open.

Following the MB1939-N6570-C02 Board schematic (https://www.st.com/resource/en/schematic_pack/mb1939-n6570-c02-schematic.pdf) the button switches to 3v3. There is a resistor R225 (10k) to GND, but marked as DNF.

So I suggest to enable an internal pull down for the button GPIO to be sure.

emmanuel_Author
Associate III
September 30, 2025

Hi mfgkw ! ,

 

Perfect, thanks for your help. Configuring BP1 with a pull-down has solved the problem !

 

Cheers

 

Emmanuel