GPIO Pins(Nucleo-H753zi)
Hello,
I’m working on a project with the NUCLEO-H753ZI board and need to connect multiple devices. I’d like to know:
1. How many GPIO pins are 5 V-tolerant for digital input?
2. How many GPIO pins are available for general use, both 3.3 V-only and 5 V-tolerant, considering the board’s default peripherals?
I want to make sure I safely use the MCU’s GPIOs for my inputs and outputs. Any guidance or reference resources would be appreciated.
Thank You!