Skip to main content
Associate II
August 6, 2024
Question

H755 Hard reset no error and soft reset in debug mode has error

  • August 6, 2024
  • 0 replies
  • 755 views

I create project with CubeMX, use Keil MDK IDE, CM7 core without user code , CM4 core has simple user code. Download code to both CM7 and CM4 then code runs correctly. Then switch to debug mode for CM4. Now, if i press Reset button on board or press Run/Stop icon on IDE then CPU runs normally, if i press Reset icon on IDE then if i press Run then will get error like this:

trieunguyen_0-1722917455133.png

Did I configure CubeMX wrong somewhere?