HELLO,
i am new to STM, i am stuck in receiving dynamic size data from HM10 to stm32f407VG over UART2 communication , i tried HAL_UART_Receive_IT(&huart2, &UART2_rxBuffer[rxIndex], 1); but not able to receive multiple char as 3rd part of this HAL_UART_Receive_IT(&huart2, &UART2_rxBuffer[rxIndex], 1); is 1 if i make it 12 then if i recive 12 char then data is visible and i want to receive any size of data string .
please help
THANKS
/* USER CODE BEGIN Header */
/**
******************************************************************************
* @file : main.c
* @brief : Main program body
******************************************************************************
* @attention
*
* <h2><center>© Copyright (c) 2024 STMicroelectronics.
* All rights reserved.</center></h2>
*
* This software component is licensed by ST under BSD 3-Clause license,
* the "License"; You may not use this file except in compliance with the
* License. You may obtain a copy of the License at:
* opensource.org/licenses/BSD-3-Clause
*
******************************************************************************
*/
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
#include <string.h>
#include"liquidcrystal_i2c.h"
//#include "stdio.h"
/* USER CODE END Includes */
/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
/* USER CODE END PTD */
/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
/* USER CODE END PD */
/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */
/* USER CODE END PM */
/* Private variables ---------------------------------------------------------*/
I2C_HandleTypeDef hi2c1;
UART_HandleTypeDef huart2;
/* USER CODE BEGIN PV */
uint8_t UART2_rxBuffer[2] = {0};//should be 4 if sending isha
#define RX_BUFFER_SIZE 100
uint8_t data1Received = 0;
uint8_t data2Received = 0;
//#define RX_BUFFER_SIZE 50
//char rxBuffer[RX_BUFFER_SIZE];
//uint8_t rxIndex = 0;
//volatile uint8_t rxComplete = 0;
//#define LED12_PIN GPIO_PIN_12
//#define LED15_PIN GPIO_PIN_15
//char Rx_data[25] = "";
/* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_USART2_UART_Init(void);
static void MX_I2C1_Init(void);
/* USER CODE BEGIN PFP */
/* USER CODE END PFP */
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
//uint8_t Data[64];
//void Delay_ms(volatile int time_ms);
//void HAL_UARTEx_RxEventCallback(UART_HandleTypeDef *huart, uint16_t Size)
//{
// if (huart->Instance == USART2)
// {
// HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12, GPIO_PIN_SET);
// //HAL_UART_Transmit(&huart2, Data, Size, 1000);
// //HAL_UART_Transmit(&huart2, Data, Size, 1000);
// }
//// else if (huart2->Instance == USART2)
//// {
////
//// //HAL_UART_Transmit(&huart1, Data, Size, 1000);
//// }
// //HAL_UART_Receive_IT(huart2, Data, 64);
// HAL_UART_Receive_IT(huart, Data, 64);
//}
//void HAL_UART_ErrorCallback(UART_HandleTypeDef *huart)
//{
// // Handle UART errors here
// // Print error message on LCD
// HD44780_Clear();
// HD44780_SetCursor(0, 0);
// HD44780_PrintStr("UART error");
//}
void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)
{
HAL_UART_Transmit(&huart2, UART2_rxBuffer, 2, 50);//
// HAL_UART_Receive_IT(&huart2, UART2_rxBuffer, 2);//should be 4 if sending data
HD44780_Clear();
HD44780_SetCursor(0,0);
HD44780_PrintStr("gio");
if (strncmp((char *)UART2_rxBuffer, "ON", 2) == 0)
{
// Turn on LED connected to pin 15
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_SET);
//data1Received = 1; // Set flag for "isha" received
//data2Received = 0; // Clear flag for "jeet" received
}
// Check if "jeet" is received
else if (strncmp((char *)UART2_rxBuffer, "OF", 2) == 0)
{
// Turn on LED connected to pin 14
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_RESET);
//HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_SET); // ID if task is simple
//data2Received = 1; // Set flag for "jeet" received// ID IF task is time taking
//data1Received = 0; // Clear flag for "isha" received // ID IF task is time taking
}
if (huart->Instance == USART2)
{
HD44780_Clear();
HD44780_SetCursor(0,0);
HD44780_PrintStr("instance");
//HD44780_Clear();
HD44780_SetCursor(0, 1);
HD44780_PrintStr("Received: ");
HD44780_PrintStr((char *)UART2_rxBuffer);
}
HAL_UART_Receive_IT(&huart2, UART2_rxBuffer, 2);//should be 4 if sending data
}
//void toggleLEDs(void)
//{
// // Toggle LED 15 if "isha" received
// if (data1Received)
// {
// HAL_GPIO_TogglePin(GPIOD, GPIO_PIN_15);
// }
//
// // Toggle LED 14 if "jeet" received
// if (data2Received)
// {
// HAL_GPIO_TogglePin(GPIOD, GPIO_PIN_14);
// }
//}
/* USER CODE END 0 */
/**
* @brief The application entry point.
* @retval int
*/
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_USART2_UART_Init();
MX_I2C1_Init();
/* USER CODE BEGIN 2 */
HAL_UART_Receive_IT (&huart2, UART2_rxBuffer, 2);
HD44780_Init(2);
HD44780_Clear();
HD44780_SetCursor(0,0);
HD44780_PrintStr("HELLO");
HAL_Delay(200);
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
// toggleLEDs(); // Toggle LEDs based on received strings
//
// // Delay for 500 milliseconds (0.5 second)
// HAL_Delay(500);
//
// // Repeat for a total of 6 times to create a 3-second toggle
// for (int i = 0; i < 6; i++)
// {
// toggleLEDs(); // Toggle LEDs based on received strings
//
// // Delay for 500 milliseconds (0.5 second)
// HAL_Delay(100);
// }
//
// // Clear the flags after 3 seconds
// data1Received = 0;
// data2Received = 0;
// if (rxComplete) {
// rxComplete = 0; // Reset flag
//
// // Process received data
// if (strcmp(rxBuffer, "hello") == 0) {
// HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12, GPIO_PIN_SET); // Turn on LED12
// HAL_Delay(1000); // Delay for 1 second
// HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12, GPIO_PIN_RESET); // Turn off LED12
// }
// else if (strcmp(rxBuffer, "hii") == 0) {
// HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_SET); // Turn on LED15
// HAL_Delay(1000); // Delay for 1 second
// HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_RESET); // Turn off LED15
// }
//
// // Clear the buffer
// memset(rxBuffer, 0, sizeof(rxBuffer));
// rxIndex = 0;
//
// // Start another reception
// HAL_UART_Receive_IT(&huart2, (uint8_t*)&rxBuffer[rxIndex], 1);
// }
// HAL_UART_Receive(&huart2,(uint8_t*)rxBuffer,RX_BUFFER_SIZE,100);
// printf(" %s\n", rxBuffer);
// if (strcmp(rxBuffer, "hello") == 0) {
// HAL_GPIO_WritePin(GPIOD, LED12_PIN, GPIO_PIN_SET); // Turn on LED12
// HAL_Delay(1000); // Delay for 1 second
// HAL_GPIO_WritePin(GPIOD, LED12_PIN, GPIO_PIN_RESET); // Turn off LED12
// }
// else if (strcmp(rxBuffer, "hii") == 0) {
// HAL_GPIO_WritePin(GPIOD, LED15_PIN, GPIO_PIN_SET); // Turn on LED15
// HAL_Delay(1000); // Delay for 1 second
// HAL_GPIO_WritePin(GPIOD, LED15_PIN, GPIO_PIN_RESET); // Turn off LED15
// }
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}
/**
* @brief System Clock Configuration
* @retval None
*/
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
/** Configure the main internal regulator output voltage
*/
__HAL_RCC_PWR_CLK_ENABLE();
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
/** Initializes the CPU, AHB and APB busses clocks
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
RCC_OscInitStruct.PLL.PLLM = 8;
RCC_OscInitStruct.PLL.PLLN = 168;
RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
RCC_OscInitStruct.PLL.PLLQ = 4;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB busses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_5) != HAL_OK)
{
Error_Handler();
}
}
/**
* @brief I2C1 Initialization Function
* @PAram None
* @retval None
*/
static void MX_I2C1_Init(void)
{
/* USER CODE BEGIN I2C1_Init 0 */
/* USER CODE END I2C1_Init 0 */
/* USER CODE BEGIN I2C1_Init 1 */
/* USER CODE END I2C1_Init 1 */
hi2c1.Instance = I2C1;
hi2c1.Init.ClockSpeed = 100000;
hi2c1.Init.DutyCycle = I2C_DUTYCYCLE_2;
hi2c1.Init.OwnAddress1 = 0;
hi2c1.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT;
hi2c1.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE;
hi2c1.Init.OwnAddress2 = 0;
hi2c1.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE;
hi2c1.Init.NoStretchMode = I2C_NOSTRETCH_DISABLE;
if (HAL_I2C_Init(&hi2c1) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN I2C1_Init 2 */
/* USER CODE END I2C1_Init 2 */
}
/**
* @brief USART2 Initialization Function
* @PAram None
* @retval None
*/
static void MX_USART2_UART_Init(void)
{
/* USER CODE BEGIN USART2_Init 0 */
/* USER CODE END USART2_Init 0 */
/* USER CODE BEGIN USART2_Init 1 */
/* USER CODE END USART2_Init 1 */
huart2.Instance = USART2;
huart2.Init.BaudRate = 9600;
huart2.Init.WordLength = UART_WORDLENGTH_8B;
huart2.Init.StopBits = UART_STOPBITS_1;
huart2.Init.Parity = UART_PARITY_NONE;
huart2.Init.Mode = UART_MODE_TX_RX;
huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE;
huart2.Init.OverSampling = UART_OVERSAMPLING_16;
if (HAL_UART_Init(&huart2) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN USART2_Init 2 */
/* USER CODE END USART2_Init 2 */
}
/**
* @brief GPIO Initialization Function
* @PAram None
* @retval None
*/
static void MX_GPIO_Init(void)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOH_CLK_ENABLE();
__HAL_RCC_GPIOA_CLK_ENABLE();
__HAL_RCC_GPIOD_CLK_ENABLE();
__HAL_RCC_GPIOB_CLK_ENABLE();
/*Configure GPIO pin Output Level */
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12|GPIO_PIN_13|GPIO_PIN_14|GPIO_PIN_15, GPIO_PIN_RESET);
/*Configure GPIO pins : PD12 PD13 PD14 PD15 */
GPIO_InitStruct.Pin = GPIO_PIN_12|GPIO_PIN_13|GPIO_PIN_14|GPIO_PIN_15;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);
}
/* USER CODE BEGIN 4 */
/* USER CODE END 4 */
/**
* @brief This function is executed in case of error occurrence.
* @retval None
*/
void Error_Handler(void)
{
/* USER CODE BEGIN Error_Handler_Debug */
/* User can add his own implementation to report the HAL error return state */
/* USER CODE END Error_Handler_Debug */
}
#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number
* where the assert_param error has occurred.
* @PAram file: pointer to the source file name
* @PAram line: assert_param error line source number
* @retval None
*/
void assert_failed(uint8_t *file, uint32_t line)
{
/* USER CODE BEGIN 6 */
/* User can add his own implementation to report the file name and line number,
tex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
/* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */
/************************ (C) COPYRIGHT STMicroelectronics *****END OF FILE****/