Skip to main content
Associate III
July 19, 2024
Question

How to Change USB Device Descriptor in Device Manager for STM32 USB CDC FS

  • July 19, 2024
  • 1 reply
  • 2487 views

Hi Team,

I'm using STM32 USB CDC FS on my custom board. In the Windows Device Manager, it shows as "STMicroelectronics Virtual COM Port (COM6)." I want to change it to display a custom name for my board. Here are my questions:

  1. How can I change the device descriptor to show a custom name in the Device Manager?
  2. Are there any licensing requirements for using a different Vendor ID (VID)?
  3. I tried changing the #define USBD_VID 1155 to a different value, but it then shows as "USB Serial Device (COM6)". Is there a specific VID I should use, or a proper way to register a custom VID?
  4. Is it possible to change name? and How

dplogiic_0-1721394022766.png

 

dplogiic_1-1721394268323.pngdplogiic_2-1721394413501.png

 

 

1 reply

Peter BENSCH
Technical Moderator
July 19, 2024

Please see this thread, which also refers to a previous one, which explaines the procedure.

Hope that helps?

Regards
/Peter