Skip to main content
Associate III
June 18, 2024
Question

How to import software FP-SNS-DATALOG2 software to S32DS IDE so I can build and flash ?

  • June 18, 2024
  • 2 replies
  • 1059 views

I have the STEVAL-STWINBX1 development board and want to import the FP-SNS-DATALOG2 software into S32DS IDE so I can build and flash.

Is this possible and if so how ?

The user manual only mentions flashing the binary file STM32CubeProgrammer, but I would like to be able to modify the software and then flash it to the board using S32DS IDE

 

2 replies

Andrew Neil
Super User
June 18, 2024
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
johngjAuthor
Associate III
June 18, 2024

I was using the wrong IDE !

I was using "S32 Design Studio" instead of STM32 Cube IDE"

johngjAuthor
Associate III
June 18, 2024

I am using a Segger J-Link Base to try and flash/debug the DATALOG2-STWIN.box application, but get the following warning...

johngj_1-1718724959595.png

johngj_0-1718724856009.png

 

If I select yes (multiple times) I then get the following error...

johngj_3-1718725040747.png

johngj_2-1718725021179.png

 

 

johngjAuthor
Associate III
June 18, 2024

Seem to have fixed it, there was no power to the board (even though the battery was connected) so I powered the board via the USB connector