Skip to main content
Associate III
August 13, 2025
Solved

How to use multiplexing port.

  • August 13, 2025
  • 1 reply
  • 214 views

Hi all.

I'm using STM32H747I-DISCO bord.

According to user manual, Pin No.1 in Pmod™ is connected to PA11/PA0.

And Pin No.1 in STMod+ is also connected to PA11/PA0.

Then can I use PA11 as USART1_CTS via Pmod™ Pin No.1, and PA0 as GPIO via STMod+  Pin No.1 concurrently?

Thanks in advance.

Best answer by MHoll.2

No You cannot, the two pins are connected together:

 

MHoll2_0-1755080695267.png

 

1 reply

MHoll.2
MHoll.2Best answer
Senior III
August 13, 2025

No You cannot, the two pins are connected together:

 

MHoll2_0-1755080695267.png