Skip to main content
Visitor II
March 5, 2025
Question

I²C SDA and SCL pins stuck at low when the module connected

  • March 5, 2025
  • 1 reply
  • 677 views

Hi everyone !

I am having problem with the I²C connection. The problem is that, normally the the SDA and SCL pins work properly (I checked it with a logic analyzer) but when I connect them to the module or sensor I use, both of them goes LOW and stay at that level. When I reset the board, the SDA goes HIGH for a really really short time and goes LOW again. I searched on the Internet for a solution but couldn't find one.

By the way, I am using STM32 H755ZI-Q Development Board and the ADS1115 ADC module. 

The things that I checked and tried so far:

The wiring is correct

The code is correct (I am just using the HAL library functions)

The I²C address is correct

The module is working (at least I used it with Arduino without any problem)

I tried it with 10K Pull-Up resistors but nothing changed.

 

As a note, I am having this problem with an other sensor either (OV7670 camera sensor) and also I tested  different copies of these sensors and modules, in a case that they can be broken. I feel like the problem is because of a fundamental thing that I missed but since I am really using the default settings and wiring, I couldn't find the reason of the problem clearly.

Do you have any idea for it ?

1 reply

AlexWEI
ST Employee
October 11, 2025

hi 

did you solved the i2c issue ? also you can try change the pull up res to 1.5K or 4.7K to try it.