Skip to main content
JanhaviDeshpande
Associate
September 12, 2024
Question

Interfacing issue

  • September 12, 2024
  • 1 reply
  • 897 views

Help needed on interfacing buzzer with L476

1 reply

Peter BENSCH
Technical Moderator
September 12, 2024

Welcome @JanhaviDeshpande, to the community!

Many details are still missing:

  • buzzer data sheet (link to the data sheet would be fine)
  • what supply voltage will the buzzer have
  • what frequencies should the buzzer emit and at what volume?
  • which waveforms should be sent to the buzzer?
  • are you planning to use an amplifier stage, if so, which one (or do you need proposals)?

Regards
/Peter

JanhaviDeshpande
Associate
September 12, 2024

First of all, Thankyou Sir for replying to the message.

Basically, using TMB12A05 active buzzer for a project based on anamoly detection based on audio. Basic functioning includes giving alert. 

Karl Yamashita
Principal
September 12, 2024

@JanhaviDeshpande wrote:

First of all, Thankyou Sir for replying to the message.

Basically, using TMB12A05 active buzzer for a project based on anamoly detection based on audio. Basic functioning includes giving alert. 


Still not enough information on what you're trying to achieve.

  • "based on audio" - So do you have something that detects this audio? Microphone? Describe what this anomaly consists of.
  • The buzzer has a frequency range of 2300+/-300H. You need to have some kind of driver for it as well, which you haven't provided any schematic.
If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source