Skip to main content
Associate II
December 13, 2025
Question

Issues with SAI I2S Loopback on Nucleo-WB55 Using SGTL5000 (DMA + Interrupts)

  • December 13, 2025
  • 0 replies
  • 465 views

Hello everyone,

I am currently working on an audio project using the Nucleo-WB55 board and the SGTL5000 codec. I am using the SAI peripheral in I2S mode to transmit and receive audio data, but I am facing an issue when testing a simple loopback setup.


My Setup

Hardware

  • Nucleo-WB55

  • SGTL5000 audio codec (not yet fully connected — initial tests are loopback)

  • SAI SD line of Block A connected directly to SD line of Block B for loopback testing

SAI Configuration

  • SAI Block A: Master, Transmit

  • SAI Block B: Synchronous Slave, Receive

  • I2S standard, 16-bit data

  • TX and RX audio buffers: 16-bit elements, each with 10 entries

  • DMA enabled for both TX and RX

  • Interrupts enabled

  • Circular DMA mode used on SAI Block B (receiver)


Test Procedure

  1. Start SAI B reception with circular DMA.

  2. Start a blocking transmission on SAI A:

     
HAL_SAI_Transmit(hsai_BlockA, buffer, sizeof(buffer), 1000);
 
  • TX SD line is physically looped back to RX SD line.


Issue Observed

  • In the RX buffer, only the first half of the data matches the transmitted data.

  • The second half always contains the same pattern of “garbage” values, not random but incorrect and consistent.

  • This happens every time under the same configuration.


Additional Doubts

1. SAI Master Clock Behavior

I’m not fully clear on when the SAI master clock (MCLK) is active:

  • Is MCLK always active after HAL_SAI_Init()?

  • Or does it only become active when a transmission/reception starts?

  • Does DMA mode affect this in any way?

2. Understanding SAI Operation

I would appreciate guidance or test ideas to:

  • Validate whether my SAI configuration is correct

  • Verify whether the issue is related to clocking, DMA alignment, buffer size, or frame configuration

  • Rule out synchronization issues between SAI A and B


Request for Help

Any suggestions on:

  • How to properly test SAI I2S loopback

  • What configurations are commonly overlooked

  • How to confirm that SAI clocks and frame sync are correct

  • How to correctly align DMA buffer sizes with SAI frame settings

would be extremely helpful.


If any additional information (CubeMX settings, code snippets, register values, schematics, etc.) would help, please let me know and I will provide it.

Thank you.
Umair Jarullah