Skip to main content
Associate III
December 19, 2024
Solved

Looking for STM32H745II ST board to evaluate ADC

  • December 19, 2024
  • 1 reply
  • 685 views

Hi,

I would like to evaluated ADC of STM32H745. I would like to have 12bit 5.12MHz dual ADC. According to my understanding, I need to use model STM32H745II in 176 pin UFBGA to obtain ADC performance. Is there any board like nucleo, which can be used for evaluation?

Best answer by mƎALLEm

@mosamasa wrote:

According to my understanding, Disco is based on STM32H745XI (240pin TFBGA). Maximum ADC rate would be only 4.38MHz.


Yes you're right according to the AN5354:

SofLit_0-1734618806165.png

But, unfortunately, there is no other ST boards for STM32H745 with other packages.

The only available ST boards for STM32H745 are with LQFP144 and TFBGA240.

1 reply

mƎALLEm
Technical Moderator
December 19, 2024
"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question."
mosamasaAuthor
Associate III
December 19, 2024

According to my understanding, Disco is based on STM32H745XI (240pin TFBGA). Maximum ADC rate would be only 4.38MHz.

mƎALLEm
mƎALLEmBest answer
Technical Moderator
December 19, 2024

@mosamasa wrote:

According to my understanding, Disco is based on STM32H745XI (240pin TFBGA). Maximum ADC rate would be only 4.38MHz.


Yes you're right according to the AN5354:

SofLit_0-1734618806165.png

But, unfortunately, there is no other ST boards for STM32H745 with other packages.

The only available ST boards for STM32H745 are with LQFP144 and TFBGA240.

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question."