my UART interrupt doesn't work
- May 3, 2025
- 4 replies
- 1800 views
Hello,
I am working on a project with a Nucleo-G431KB. I am using UART1 to receive GPS data (LEA-6S module, 9600 baud, 3.3V) on pin PB7 (RX), and I send data to a LoRa module (Ebyte E32868T20 module, 3.3V, 9600 baud too) on PB6 (TX).
I configured UART1 in asynchronous mode with interrupts enabled (USART1 global interrupt active).
In my code, I call HAL_UART_Receive_IT(&huart1, &recep, 1) at startup, and I relaunch HAL_UART_Receive_IT at the end of HAL_UART_RxCpltCallback().
The GPS sends data correctly (tested with a direct connection) and the lora module works too (tested by sending text every 3 seconds), but on the Nucleo, the UART interrupt never seems to trigger.
I give you my main.c and my .ioc file
Any idea what could block the UART RX interrupt on the G431KB?
Thanks!