Need for series resistors for OCTOSPI on STM32H7- and U5-boards?
Hi,
I am working with some custom boards for H7 and U5-series.
The board schematics for STM32H735IG-DK and STM32U5A9-DISC shows both boards are using the same OCTO SPI but only the H7-board is using series resistors of 33 ohms for the all the data lines.
In order to minimize reflections and match the transmission’s 50 ohms impedance, I have understood it as series resistor values should be chosen as: R_value = 50 ohm - MCU_impedance. In such case one would assume the H7-series has an output impedance of about 20 ohms and the U5-series about 0 ohms.
- Is this a correct assumption / best practice?
- Are series resistors needed/reccomended on a U5-design?
- Is output impedance documented somewhere? (could not find it in ref. manuals for memory bus)
Thanks for any hints