Skip to main content
Associate II
June 14, 2024
Solved

Nucleo-F767ZI must reset after power ON

  • June 14, 2024
  • 2 replies
  • 2473 views

Hello everyone, my programme on Nucleo-F767ZI do not run when I power ON by external power supply. I force to press reset button or power supply st-link by usb cable.

I searched some solutions such as: BOOT0 to GND; or turn on bit POR = 1 in RCC_CSR, but nothing worked. 

I don't want to use external circuit to reset.

Anyone can share with me some useful solutions to solve this issue?

Best answer by mƎALLEm

So can I remove SB3 and SB111 like 3.3V?


No, so you need to read the first section (VIN/E5V) and apply the described power sequence procedure.

2 replies

AScha.3
Super User
June 14, 2024

Hi,

so your nucleo is running, if connecting st-link -> USB ?

But without power on st-link - not ?

Then look , what you get, if st-link not powered:

AScha3_0-1718345216792.png

Clk is coming from st-link , so you have to power the st-link, to get the 8MHz clk, 

or set solder bridges + a crystal connected to F767,

or use only internal HSI clk in your program.

+

Boot0 at gnd , is always needed, if you dont want to start the internal bootloader.

+

NRST has to be separated from st-link, if you dont power it; so power st-link, even if you dont use it - 

or separate the F767 reset from not powered st-link.

Just look at the circuit of your board, to see, what to do .

https://www.st.com/resource/en/schematic_pack/nucleo_144pins_sch.zip

 

"If you feel a post has answered your question, please click ""Accept as Solution""."
ManhPhamAuthor
Associate II
June 14, 2024

Thanks for your advice.

Using clk HSI make the timer run incorrectly in my programme. Best option is supply power for st-link, I don't want to supply through the Micro USB port. 

Could I external supply power for st-link by jumper or other pin ? Which pin, pls help?

mƎALLEm
Technical Moderator
June 14, 2024

Hello,

Please refer to the UM1974 page 23:

SofLit_0-1718358483613.png

For 3.3V power supply: you need to remove SB3 and SB111 to disconnect ST-LINK from the main MCU because it's keeping resetting it.

 

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question."
Explorer II
January 20, 2026

this solved the problem for me:

https://community.st.com/t5/stm32-mcus-boards-and-hardware/nucleo-f767zi-external-power-start-up-problem/m-p/714804#M21087

here in short:

PROBLEM:

The clock for the STM32 is provided by the on board debugger. This clock signal is generated about 2 seconds after the board is power, after which a reset takes effect. By default HSE Startup Timout Value is 100ms, so it timeouts before the clock is available → the board doesn’t start.

that solves it:

  1. If you don't care to much of startup time increase timeout for the HSE to wait for MCO (RCC -> Parameter Settings -> HSE Startup Timout Value (ms))
  2. use the internal clock HSI (if you don’t need accurate clock)
  3. use external oscillator (X3, HSE) - soldering needed

thanks to Elec in the OG post on stack overflow and Rubb to extend it.