Skip to main content
Associate III
October 28, 2025
Question

[NUCLEO-H753ZI + X-NUCLEO-GNSS1A1] USART2 IRQ triggered continuously, no GNSS NMEA output

  • October 28, 2025
  • 0 replies
  • 144 views

Hi everyone,


I am using the X-NUCLEO-GNSS1A1 (Teseo-LIV3F) with a NUCLEO-H753ZI board.
The UART2 interrupt is working correctly, verified by "[GNSS_RX] UART RX Callback triggered",
but the GNSS module does not send any "$GPGGA" or NMEA sentences.
Only binary-like data such as "E" or 0x00 are received.
The FSM remains in fsm_discard state and never detects the "$" character.

Hardware setup:

  • NUCLEO-H753ZI

  • X-NUCLEO-GNSS1A1 (Teseo-LIV3F)

  • STM32CubeIDE 1.19.0, X-CUBE-GNSS1 middleware

  • UART2 via Zio connector 

  • Jumpers: Closed: J3, J13, J5, J9, J12, J11, J14, J15; Open: J2, J4, J6, J7, J8, J10

  • GNSS board green LED is ON (steady)

Software behavior:
Initialization appears successful:
[BSP_INIT] MX_USART2_UART_Init SUCCESS
[TESEO_INIT] Initialization completed successfully
[GNSS_CB] UART callbacks registration done

UART2 interrupt log:
USART2 IRQ triggered
[GNSS_RX] UART RX Callback triggered
[FSM] discard: 0x00 (.E

 

I would appreciate any guidance on this issue.

I also attached my set-up and Project File.

 

HANITALY_0-1761662924374.jpegHANITALY_1-1761662930130.jpeg