Associate III
October 6, 2025
Solved
NUCLEO-H7S3L8 HSE times out
- October 6, 2025
- 7 replies
- 1035 views
I am trying to set up a basic USB project on a NUCLEO-H7S3L8. It works okay with the HSI, but I need the HSE. I can see that the board has a 24MHz crystal fitted and resistors on SB14 and SB15. It's unmodified from the factory.
HAL_RCC_OscConfig() always returns with a timeout when trying to activate the HSE. I've tried various settings but can't get it to work.
I have attached my .ico file. The code is just what CubeMX generates. Thanks.