Skip to main content
Senior II
July 14, 2025
Question

Nucleo-L433RC-P board - difficulty with flashing and debugging

  • July 14, 2025
  • 3 replies
  • 349 views

I am using the Nucleo-L433RC-P board but having difficulty flashing and debugging.  9 out of 10 times I get the following error...

freeflyer_0-1752489543394.png

STMicroelectronics ST-LINK GDB server. Version 7.11.0
Copyright (c) 2025, STMicroelectronics. All rights reserved.

Starting server with the following options:
 Persistent Mode : Disabled
 Logging Level : 1
 Listen Port Number : 61234
 Status Refresh Delay : 15s
 Verbose Mode : Disabled
 SWD Debug : Enabled
 InitWhile : Enabled

Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
 -------------------------------------------------------------------
 STM32CubeProgrammer v2.20.0 
 -------------------------------------------------------------------



Log output file: C:\Users\JOHNLI~1\AppData\Local\Temp\STM32CubeProgrammer_a47444.log
ST-LINK SN : 066BFF323355373043142426
ST-LINK FW : V2J46M31
Board : NUCLEO-L433RC-P
Voltage : 3.27V
SWD freq : 4000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x435
Revision ID : Rev Z
Device name : STM32L43xxx/STM32L44xxx
Flash size : 256 KBytes
Device type : MCU
Device CPU : Cortex-M4
BL Version : 0x91



Opening and parsing file: ST-LINK_GDB_server_a47444.srec


Memory Programming ...
 File : ST-LINK_GDB_server_a47444.srec
 Size : 41.44 KB 
 Address : 0x08000000


Erasing memory corresponding to segment 0:
Erasing internal memory sectors [0 20]
Download in Progress:


File download complete
Time elapsed during download operation: 00:00:01.464



Verifying...




Error: Data mismatch found at address 0x0800A4E1 (byte = 0xC0 instead of 0x00)


Time elapsed during verifying operation: 00:00:00.277


Error: Download verification failed


Encountered Error when opening C:\ST\STM32CubeIDE_1.18.1\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_2.2.200.202503041107\tools\bin\STM32_Programmer_CLI.exe
Error in STM32CubeProgrammer
Shutting down...
Exit.

Methods I use to try and get it working is:

  • Disabling 5V power (see setup diagram below),
  • Disconnecting the USB
  • Restarting STMCubeIDE
  • Deleting the Debug folder
  • Disconnecting other interface boards (see setup diagram below)

Then 1/10 times it will suddenly work.

This problem originally started when I tried to retarget the MCU from an STM32L433RCTxP to STM32L433RCTx.

I did this by editing the .ioc file and changing any reference of STM32L433RCTxP to STM32L433RCTx.

I have since gone back to the original MCU used on the board (i.e. STM32L433RCTxP), but having great difficulty in flashing and debugging.

I even created a new, clean project for the Nucleo-L433RC-P board, but the issue still exists.

I have other interface boards connected to the Nucleo-L433RC-P board and have tried disconnecting some of these in case they are interfering with the operation.  Sometimes it makes a difference, but other times it does not, so it could just be coincidence. 

Below is my setup...

freeflyer_3-1752490125921.png

 

 

For example, the audio amplifier is powered by the 5V SMPS, but even when the SMPS is disabled, the +3.3V from the Nucleo-L433RC-P board (which is used for I2CVDD pin and IC2 pull up resistors) seems to somehow power the amplifier (LED on and audio plays).

 

freeflyer_5-1752490454219.png

 

 

Why am I having such difficulty flashing and debugging and how to I resolve it ?

Is the Nucleo-L433RC-P board damaged or are my interface boards causing an issue ?

 

3 replies

freeflyerAuthor
Senior II
July 14, 2025

It wouldn't have anything to do with the external SMPS would it ?

A clean project for the Nucleo-L433RC-P board uses the following pin out...

freeflyer_0-1752517667016.png

 

But my project does not use the external SMPS and I have re-assigned the pins:

 

  • PA4
    • Was a digital output (SMPS_EN)
    • Now an analogue output (DAC1_OUT1)
  • PA5
    • Was a digital output (SMPS_V1)
    • Still a digital output (STATUS_LED)
  • PA6
    • Was a digital input (SMPS_PG)
    • Still a digital input (SPI MISO)
  • PA7
    • Was a digital output (SMPS_SW)
    • Still a digital output (SPI MOSI)

 

freeflyer_1-1752517758896.png

 

Could these changes have caused any damage ?

Because it still doesnt flash or debug even if I swtich to a clean project for the Nucleo-L433RC-P board 

Can the Nucleo-L433RC-P board be used without the external SMPS ?

 

freeflyerAuthor
Senior II
July 14, 2025

I have removed JP8 on the Nucleo-L433RC-P board which disables the external SMPS.

Now I am able to flash and debug, so I am wondering whether reassigning the pins could have damaged the SMPS ?

I wont be using the SMPS on my custom PCB so wont have that issue, but could this be the cause of the problems I have been having ?

freeflyerAuthor
Senior II
July 14, 2025

Spoke too soon :(

It stopped working again...

I have ordered a replacement board but wary that I dont want to damage it in case I damaged the original one