Skip to main content
Visitor II
April 16, 2026
Question

PA1 Voltage Level in Reset State – Nucleo-F446ZE

  • April 16, 2026
  • 3 replies
  • 94 views
Hello,
 
While using the Nucleo-F446ZE, I observed that pin PA1 remains at approximately 2.6 V during reset, even when an external pull-down resistor is applied. On this development board, PA1 can be configured as the RMII Reference Clock. However, I have removed SB13, so this function should be disconnected and no longer influence the pin. Given that no internal or external circuitry should be driving this pin and considering that an external pull-down resistor is present I would expect PA1 to be held at 0 V during reset.
 
Why the pin is not pulled low in this condition?

3 replies

Andrew Neil
Super User
April 16, 2026

Have you checked the schematics to be sure that there isn't anything still connected - even after removing SB13 ?

What pull-down value are you using? Are you sure it is well-connected?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
mƎALLEm
Technical Moderator
April 16, 2026

Hello @usinfi and welcome to the ST community,

Nothing special on PA1:

mALLEm_0-1776351261537.png

Check again SB13 is well removed/unsoldered and you haven't nothing connected externally to it.

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question."
TDK
Super User
April 16, 2026

Where exactly are you measuring it? It's not exposed on a header.

If you are measuring on CN9 pin 13, you will need to close SB11 which is open by default.

TDK_0-1776352319627.png

 

"If you feel a post has answered your question, please click ""Accept as Solution""."
mƎALLEm
Technical Moderator
April 16, 2026

Not exposed on the Zio connector 

mALLEm_0-1776353006797.png

But exposed on CN11 (Morpho connector not mounted by default on the board):

mALLEm_1-1776353081895.png

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question."