Pin-out of STM32H723 vs. STM32H7 Nucleo-144 boards
Dear all,
I am trying to make sense of the pin descriptions / pin-mapping of the STM32H7 Nucleo-144 boards, vs. the MCU STM32H723 which it is equiped with.
User manual UM2407 (rev. 4) of the board reads:
- pin PA3 has function ADC12_INP15
- pin PC0 has function ADC123_INP10
- pin PC3 has function ADC12_INP13
- pin PB1 has function ADC12_INP5
- pin PC2 has function ADC123_INP12 (i.a.)
- pin PF10 has function ADC3_INP6 (i.a.)
However, in the reference manual RM0468 (rev. 3) of the MCU:
- ADC12_INP15 appears only in Figure 163 for ADC2 connectivity; how come is it called ADC12?
- ADC123_INP10 doesn't appear at all in the .pdf. What could the reason be?
- ADC12_INP13 appears both in Figure 162 for ADC1 and in Figure 153 for ADC2, this is plausible
- ADC12_INP5 appears in Figure 162 for ADC1 and also in Figure 153 for ADC2, this is plausible
- ADC123_INP12 doesn't appear at all in the .pdf. What could the reason be?
- ADC3_INP6 appears both in Figure 231 for ADC3, this is also plausible
Many thanks in advance