Skip to main content
Associate III
September 15, 2024
Question

Programming STM32H745i with St-link v2

  • September 15, 2024
  • 1 reply
  • 921 views

When programming STM32H745i with St-link v2 I notice that the display does not turn on, only LD2 flashes red and can not load the code giving the following message:

stmcubeide v1.16.0 upgraded stlink v2 without problems and recognizes it well.

Maximiliano_0-1726440766400.png

 

 

In the schematic I did not seem to see any jumper that has to do with the power supply of the st-link.

Did I miss to do something besides connecting (SWDIO,GND,SWCLK,3.3V)?

I even tried to power it by USB and connect the st-link v2 without the 3.3V but it didn't work either.

1 reply

Tesla DeLorean
Guru
September 16, 2024

Is this an ST-LINK on a NUCLEO board?

Disconnect the local target, two jumpers.

Try with STM32 Cube Programmer directly. 

Check Target is properly powered and functional. Check voltage at VCAP. 

Share circuit diagram for your board

 

Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..
Associate III
September 16, 2024

It is an external stlink to the board.Sorry I am new to the board and do not understand your instructions.

Attached is the schematic I consulted.