Question
SPI problem on STM32H7
Hello, I’m having a problem with a board I’m developing based on the STM32H747BIT6. The issue is related to SPI communication.
When I connect any device to the SPI bus, the signal level drops from 3.3 V to around 1.5 V. I have tested different SPI peripherals, but they all show the same behavior.
Could this be related to the drive strength or power capability of a specific pin?