Question
ST‑LINK V3 Minie connects to STM32F100RBT6B Discovery but not to my custom board
- December 1, 2025
- 2 replies
- 695 views
I’m using an ST‑LINK V3 Minie with an STM32F100RBT6B Discovery board (which also has an STM32F103C8T6), and it works perfectly. However, when I connect the same ST‑LINK V3 Minie to my custom board that uses the same STM32F100RBT6B chip, it fails to connect.
I’ve wired VCC (VTref), GND, NRST, TMS/SWDIO, and TCK/SWCLK exactly as specified.
Black - Ground
White - Vcc
Yellow - Reset
Blue - Clock
Purple - TMS
On the Discovery board this setup works fine, but on my custom board the debugger cannot establish communication.
Could anyone suggest what additional checks I should perform on the custom board?