Skip to main content
CGadg
Associate III
October 25, 2024
Question

ST-link Vapp highest series resistor

  • October 25, 2024
  • 1 reply
  • 918 views

What is the highest value series resistor which can be put into the ICSP Vapp pin a design?

It being connected to VDD and presenting a risk of harm if connected wrongly. 

I can spend time testing this but would prefer to know if this has a definite value.

1 reply

CGadg
CGadgAuthor
Associate III
October 30, 2024

I tested 5k, errors only. 2.5k seemed OK, and I only need 330R so that will do.

I'll leave this open for further comments. My programmer is the ST-LINK V2

Andrew Neil
Super User
October 30, 2024
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
CGadg
CGadgAuthor
Associate III
October 30, 2024

It's a genuine one