Question
Starting USB device in STM32H753I Eval 2 development board
- July 26, 2024
- 1 reply
- 873 views
Hi
We are trying to test USB Device - CDC standalone example with STM32H753i eval2 board. Our main.c code is enclosed herewith,
Issue: if we call USBD_START() function in the main the LED Toggling code which is written below is not executing.
In Debug mode the system hangs at HAL_GPIO_WritePin.
If USBD_Start call is Commented, then Toggling of LED Observed in both run and debug modes.
Clock Configuration can be verified with the code.
Kindly share your suggestions.