STLink not appearing in Device Manager
I installed stsw-link009 on my pc so I could use the STLinkv3. The PC did not see the STLink-v3. I then installed STM32Cubeprogrammer thinking that would fix the stlink driver issue but when I look under devices USB in the device manager I can not see the stlinkv3 anywhere and the STM32CubeProgrammer doesn't see it either. The same stlinkv3 works on other pcs. Since I can't see it on my pc I can't right click it to uninstall the driver so I am not sure what to do next.