STLink V3 MINIE won't connect to STM32U0 target; V2 and V3_SET connect OK
I have the following original debuggers:
Stlink V2
Stlink V3_SET
Stlink V3_MINIE (2 pieces)
I was recently testing a simple board with an STM32U083 (powered by 3.3V) and found that two Stlink V3 MINIE units could connect to the MCU. Meanwhile, both the V2 and V3_SET work without any issues.
I observed that after connecting (SWDIO,SWCLK,VDD,GND) to the powered MCU, both the V2 and V3_SET leave SWDIO at 3.3V (pull-up in the MCU) and SWCLK at 0V (pull-down in the MCU). Whereas the MINIE maintains a 3.3V level on both SWDIO and SWCLK. Out of curiosity, I connected an external 10k pull-down resistor to both SWDIO and SWCLK and observed that SWDIO drops (which is fine), but SWCLK does not, meaning that the Stlink V3 MINIE actively holds SWCLK at 3.3V.
Am I doing something wrong, or are both MINIE boards defective?
Best regards,
Michal Dudka