Skip to main content
Associate
July 3, 2025
Question

STLINK V3 USB issue

  • July 3, 2025
  • 5 replies
  • 600 views

Hello all,

 

I've been using my STLINK V3 successfully for around half a year until it suddenly stopped working from one day to the next. When connecting it to the PC (no target) the green light is on and the red light if flashing forever. It does not turn orange like described in the manual, neither switch to constant red, as it was before. Windows it not recognizing it as an USB device at all (the first two times it showed something like unknown device, but never again since).

My setup works with another STLINK V3 so I would exclude cable, USB port issues or similar. 

 

Any idea, what the issue here is, or how to fix it?

5 replies

TDK
Super User
July 3, 2025

If red light is flashing, it indicates the chip is trying to connect but enumeration is failing. Typically this is due to a bad cable, perhaps a power-only cable. It could also be that your PC doesn't like that device for some USB stack reason. Rebooting can sometimes fix this.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Associate
July 3, 2025

I tried already several cables ans USB ports, even another PC, but the behavior is the same. As mentioned above on the same PC, same USB port, same cable my ST Links used to work and another ST link is still working perfectly. That's why I concluded, that something with the actual STLink HW must be wrong.

Andrew Neil
Super User
July 3, 2025
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Associate
July 4, 2025

I connected the STLink to a Linux PC and got the following log. I hope this helps to determine the issue.

 

[ 99.227313] usb 1-2: new full-speed USB device number 5 using xhci_hcd
[ 99.342252] usb 1-2: device descriptor read/64, error -71
[ 99.563204] usb 1-2: device descriptor read/64, error -71
[ 99.786283] usb 1-2: new full-speed USB device number 6 using xhci_hcd
[ 99.901289] usb 1-2: device descriptor read/64, error -71
[ 100.123345] usb 1-2: device descriptor read/64, error -71
[ 100.232439] usb usb1-port2: attempt power cycle
[ 100.612313] usb 1-2: new full-speed USB device number 7 using xhci_hcd
[ 100.612520] usb 1-2: Device not responding to setup address.
[ 100.816448] usb 1-2: Device not responding to setup address.
[ 101.024232] usb 1-2: device not accepting address 7, error -71
[ 101.024327] usb 1-2: WARN: invalid context state for evaluate context command.
[ 101.138232] usb 1-2: new full-speed USB device number 8 using xhci_hcd
[ 101.138438] usb 1-2: Device not responding to setup address.
[ 101.344489] usb 1-2: Device not responding to setup address.
[ 101.552070] usb 1-2: device not accepting address 8, error -71
[ 101.552168] usb 1-2: WARN: invalid context state for evaluate context command.
[ 101.552279] usb usb1-port2: unable to enumerate USB device

AScha.3
Super User
July 4, 2025

So you have a bad contact on one USB data line - or you killed this V3 (maybe static discharge, the "usual way").

"If you feel a post has answered your question, please click ""Accept as Solution""."
Technical Moderator
July 21, 2025

Hi @phil_spobu 

Given the symptoms and error logs, the USB interface hardware in the STLINK V3 is probably faulty.

  1. Check the PCB around the USB connector for cracked solder joints or lifted pads. If possible, gently reflow the USB connector solder joints with a soldering iron to restore good contact.
  2. Upgrade or reflash the STLINK firmware using STM32CubeProgrammer, as firmware corruption can sometimes cause enumeration issues.
  3. If these steps do not resolve the issue, the most practical solution would be to replace the STLINK V3 device.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.Best regards,FBL
Associate
July 29, 2025

@FBL wrote:

2. Upgrade or reflash the STLINK firmware using STM32CubeProgrammer, as firmware corruption can sometimes cause enumeration issues.


Is there any manual for that? Which interface shall be used, where do I get the firmware from?

TDK
Super User
July 29, 2025

The only way to update firmware is using ST tools. If the programmer can't connect at all, no chance of that happening.

TDK_0-1753795925540.png

 

"If you feel a post has answered your question, please click ""Accept as Solution""."
Associate
July 29, 2025

OK. I thought I would be able to flash with another ST Link directly over JTAG/ SWD interface. I was wondering, if this is available on one of the connectors. 

As USB is not recognized at all I cannot use the standard way of flashing the firmware.