Skip to main content
debugging
Lead
December 6, 2024
Question

STLINK-V3MODS - UART RX/TX are reversed compared to VUART - Please help ?

  • December 6, 2024
  • 3 replies
  • 1930 views

continuing from this : https://community.st.com/t5/stm32-mcus-boards-and-hardware/stlink-v3mods-uart-api/td-p/747740

Finally found the reason why could not get data from STLINK V3-MODS from the 2nd UART

Compared to the VUART the UART RX/TX pins are reversed.

Could ST please issue a firmware fix for this ? (otherwise need gerber out new boards !)

I suspect that the  designer of the V3MOD intended the VUART port as a DCE for UUT that normally act like a DTE, while the UART port on the V3MOD acted like an DTE. if that so then that should be clearly documented , right now that isn't and thus causes my V3MOD board UART port not to work with a UUT (which is a DTE). without a firmware fix, My board need to be relayout. Would really like a confirmation as this same question also applies to the RTS/CTS pins are they configured as DCE or DTE ? Could ST please clarify the exact intent how these ports supposed to be used and are configured in  the firmware ?

 

 

 

3 replies

debugging
debuggingAuthor
Lead
December 15, 2024

Hello ST, do you have a confirmation about this ? Checked my schematic and can't find a mistake

Tesla DeLorean
Guru
December 15, 2024

Open an On-Line Support Request, in the OLS, or work with your FAE

https://www.st.com/resource/en/hw_model/stlink-v3mods_voltage-translator_reference-design.pdf

STLK_VCP_RX (OUT)

STLK_VCP_TX (IN)

Bridge_UART_RX (IN)

Bridge_UART_CTS (IN)

Bridge_UART_TX (OUT)

Bridge_UART_RTS (OUT)

At a board level UART perhaps you can use the ADV_FEATURES to switch the RX/TX if your STM32 Target supports that.

 

Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..
debugging
debuggingAuthor
Lead
December 18, 2024

Thanks for pointing this out. It's seems it is the VCP that is reversed from a default UART setting.

As this is designed as is, it would have been nice not to have to find this out by the schematic .

Recommendations to ST for UM2502 

- Section 8.4 : Add a note or specify the direction of the UART/VCP of the pins.

- Section 8.4.4: Add a note to use the ST Programs tools to enable the UART

 

Unfortunately it seems this older STM32 (F4) seems not to have support for the swap.

'UART_HandleTypeDef' {aka 'struct __UART_HandleTypeDef'} has no member named 'AdvancedInit'

 

 

Mike_ST
Technical Moderator
December 19, 2024

Hello,

>> Recommendations to ST for UM2502 

>> - Section 8.4 : Add a note or specify the direction of the UART/VCP of the pins.

>> - Section 8.4.4: Add a note to use the ST Programs tools to enable the UART

Thank you for your suggestion, so I wanted to check whether there is an improvement that could be done, but I don't see a section 8 in UM2502.

Could you upload the document you're talking about ?

 

debugging
debuggingAuthor
Lead
December 21, 2024

As attached. I noted there is a rev 2 that has major changes and moved this to section. P.S please also make it clear where to get the tools to change the function to UART, in which package/software download.