Skip to main content
IVent.1
Senior
March 18, 2025
Solved

stlinkv3 and stlinkv2isol

  • March 18, 2025
  • 1 reply
  • 424 views

I have this 2 programmers, stlinkv2isol and stlinkv3.

With the first, I'm able to program and debug my board. But with the second, no, I received a message like this

 

ST-LINK SN : 0050002E3331510633323639

ST-LINK FW : V3J13M4B5S1

Board : STLINK-V3SET

Voltage : 1.78V

Error: No STM32 target found! If your product embeds Debug Authentication, please perform a discovery using Debug Authentication

2nd connect tentative with frequency (8MHz)

ST-LINK SN : 0050002E3331510633323639

ST-LINK FW : V3J13M4B5S1

Board : STLINK-V3SET

Voltage : 1.77V

Error: ST-LINK error (DEV_CONNECT_ERR)

Encountered Error when opening C:\ST\STM32CubeIDE_1.16.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_2.1.400.202404281720\tools\bin\STM32_Programmer_CLI.exe

Error in STM32CubeProgrammer

Shutting down...

Exit.

I'm using the JTAG connector of stlinkv3 (CN2).

Thank you.

Best answer by Peter BENSCH

Your target voltage appears to be around 1.8V, which is OK for ST-LINK/V2-ISOL, but no longer for a pure STLINK-V3SET.

Without the B-STLINK-VOLT extension, STLINK-V3SET is intended for a target VCC of 3-3.6V, while ST-LINK/V2-ISOL operates between 1.65-3.6V.

Regards
/Peter

1 reply

Peter BENSCH
Peter BENSCHBest answer
Technical Moderator
March 18, 2025

Your target voltage appears to be around 1.8V, which is OK for ST-LINK/V2-ISOL, but no longer for a pure STLINK-V3SET.

Without the B-STLINK-VOLT extension, STLINK-V3SET is intended for a target VCC of 3-3.6V, while ST-LINK/V2-ISOL operates between 1.65-3.6V.

Regards
/Peter