Skip to main content
Associate
July 28, 2024
Solved

STM32 Cube Programmer behaves as if programs do not exist

  • July 28, 2024
  • 2 replies
  • 1125 views

It looped at a location deprived of access, waited a second, and returned to the same action. I thought STM32 was about programming.

Best answer by golvict

Point taken. My problem was the invasive fashion of the installation. I appreciate that STM32CubeProgrammer cleaned the area and even changed some things without asking or alerting - it felt a positive impact. But I cannot consider this an installation: it took 48 hours, as long as I could bear a CPU-hog and whirling circle-icon sticking to the mouse cursor. Then I terminated STM32CubeProgrammer. I couldn't work.

2 replies

AScha.3
Super User
July 28, 2024

Which cpu ?

Which st-link ?

+

Show pic, what CubePrg. telling:

like this

AScha3_0-1722186760189.png

 

"If you feel a post has answered your question, please click ""Accept as Solution""."
TDK
Super User
July 28, 2024

I think this is a complaint about the forum software, not the STM32 hardware, but it's hard to tell with such limited info.

Some links are broken, yes, but complaining without describing what you're looking for isn't going to get you anywhere. We're not mind readers.

"If you feel a post has answered your question, please click ""Accept as Solution""."
golvictAuthorBest answer
Associate
August 1, 2024

Point taken. My problem was the invasive fashion of the installation. I appreciate that STM32CubeProgrammer cleaned the area and even changed some things without asking or alerting - it felt a positive impact. But I cannot consider this an installation: it took 48 hours, as long as I could bear a CPU-hog and whirling circle-icon sticking to the mouse cursor. Then I terminated STM32CubeProgrammer. I couldn't work.