Skip to main content
Associate
September 10, 2024
Question

STM32-NUCLEO-F411RE using two I2S result in loop in I2S_WaitFlagStateUntilTimeout()

  • September 10, 2024
  • 1 reply
  • 1027 views

Hi, it's my first time using a STM32-NUCLEO-F411RE (actually the STM32 in general) and im trying to get some audio using a i2s MEMS microphone, modifying it using the DSP, and outputting it on another i2s.
The microphone is working, and im turning a led on and off whenever it reads an amount of sounds over a threshold, dps is working fine aswell, however, when i turn the other i2s on (deactivating the SPI on the Cube IDE and activating the other i2s) the microphone is going in a loop as soon as i use HAL_I2S_Receive, going in a loop on :

 

 

 

static HAL_StatusTypeDef I2S_WaitFlagStateUntilTimeout(I2S_HandleTypeDef *hi2s, uint32_t Flag, FlagStatus State,
 uint32_t Timeout)
{
 uint32_t tickstart;

 /* Get tick */
 tickstart = HAL_GetTick();

 /* Wait until flag is set to status*/
 while (((__HAL_I2S_GET_FLAG(hi2s, Flag)) ? SET : RESET) != State)
 {
 if (Timeout != HAL_MAX_DELAY)
 {
 if (((HAL_GetTick() - tickstart) >= Timeout) || (Timeout == 0U))
 {
 /* Set the I2S State ready */
 hi2s->State = HAL_I2S_STATE_READY;

 /* Process Unlocked */
 __HAL_UNLOCK(hi2s);

 return HAL_TIMEOUT;
 }
 }
 }
 return HAL_OK;
}

 

 

 

 The i2s clock is set at 96MHz, i tried changing it but nothing worked (and it works when i use only one i2s).

 

My code is:

 

 

 

int main(void)
{

 HAL_Init();

 SystemClock_Config();

 PeriphCommonClock_Config();


 MX_GPIO_Init();
 MX_ADC1_Init();
 MX_I2S3_Init();
 MX_I2S2_Init();

 int above_threshold_count = 30;

 while (1)
 {
	 HAL_I2S_Receive(&hi2s2, (uint16_t *)audio_buffer, FILTER_ORDER, HAL_MAX_DELAY);
	 int noiseType = 0; 
	 float avgAmplitude = 0.0f;
	 if (avgAmplitude > AUDIO_THRESHOLD) {
	 above_threshold_count = DEBOUNCE_COUNT;
	 HAL_GPIO_WritePin(LD2_GPIO_Port, LD2_Pin, GPIO_PIN_SET); 

	 generateNoise(masking_output, FILTER_ORDER, MASKING_VOLUME, noiseType);

	 HAL_I2S_Transmit(&hi2s3, (uint16_t *)masking_output, FILTER_ORDER, HAL_MAX_DELAY);
	 } else {
	 above_threshold_count -= 1;
	 if (above_threshold_count <= 0) {
	 HAL_GPIO_WritePin(LD2_GPIO_Port, LD2_Pin, GPIO_PIN_RESET); // Turn off LED
	 }

 }
}
}

void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

 /** Configure the main internal regulator output voltage
 */
 __HAL_RCC_PWR_CLK_ENABLE();
 __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE2);

 /** Initializes the RCC Oscillators according to the specified parameters
 * in the RCC_OscInitTypeDef structure.
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
 RCC_OscInitStruct.HSIState = RCC_HSI_ON;
 RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
 RCC_OscInitStruct.PLL.PLLM = 16;
 RCC_OscInitStruct.PLL.PLLN = 336;
 RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV4;
 RCC_OscInitStruct.PLL.PLLQ = 7;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;

 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2) != HAL_OK)
 {
 Error_Handler();
 }
}

/**
 * @brief Peripherals Common Clock Configuration
 * @retval None
 */
void PeriphCommonClock_Config(void)
{
 RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};

 /** Initializes the peripherals clock
 */
 PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_I2S;
 PeriphClkInitStruct.PLLI2S.PLLI2SN = 192;
 PeriphClkInitStruct.PLLI2S.PLLI2SR = 2;
 if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
 {
 Error_Handler();
 }
}

/**
 * @brief ADC1 Initialization Function
 * None
 * @retval None
 */
static void MX_ADC1_Init(void)
{

 /* USER CODE BEGIN ADC1_Init 0 */
 /* USER CODE END ADC1_Init 0 */

 ADC_ChannelConfTypeDef sConfig = {0};

 /* USER CODE BEGIN ADC1_Init 1 */
 /* USER CODE END ADC1_Init 1 */

 /** Configure the global features of the ADC (Clock, Resolution, Data Alignment and number of conversion)
 */
 hadc1.Instance = ADC1;
 hadc1.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV4;
 hadc1.Init.Resolution = ADC_RESOLUTION_12B;
 hadc1.Init.ScanConvMode = DISABLE;
 hadc1.Init.ContinuousConvMode = DISABLE;
 hadc1.Init.DiscontinuousConvMode = DISABLE;
 hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
 hadc1.Init.ExternalTrigConv = ADC_SOFTWARE_START;
 hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT;
 hadc1.Init.NbrOfConversion = 1;
 hadc1.Init.DMAContinuousRequests = DISABLE;
 hadc1.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
 if (HAL_ADC_Init(&hadc1) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure for the selected ADC regular channel its corresponding rank in the sequencer and its sample time.
 */
 sConfig.Channel = ADC_CHANNEL_0;
 sConfig.Rank = 1;
 sConfig.SamplingTime = ADC_SAMPLETIME_3CYCLES;
 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN ADC1_Init 2 */
 /* USER CODE END ADC1_Init 2 */

}

/**
 * @brief I2S2 Initialization Function
 * None
 * @retval None
 */
static void MX_I2S2_Init(void)
{

 /* USER CODE BEGIN I2S2_Init 0 */
 /* USER CODE END I2S2_Init 0 */

 /* USER CODE BEGIN I2S2_Init 1 */
 /* USER CODE END I2S2_Init 1 */
 hi2s2.Instance = SPI2;
 hi2s2.Init.Mode = I2S_MODE_MASTER_RX;
 hi2s2.Init.Standard = I2S_STANDARD_PHILIPS;
 hi2s2.Init.DataFormat = I2S_DATAFORMAT_16B;
 hi2s2.Init.MCLKOutput = I2S_MCLKOUTPUT_DISABLE;
 hi2s2.Init.AudioFreq = I2S_AUDIOFREQ_8K;
 hi2s2.Init.CPOL = I2S_CPOL_LOW;
 hi2s2.Init.ClockSource = I2S_CLOCK_PLL;
 hi2s2.Init.FullDuplexMode = I2S_FULLDUPLEXMODE_DISABLE;
 if (HAL_I2S_Init(&hi2s2) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN I2S2_Init 2 */
 /* USER CODE END I2S2_Init 2 */

}

/**
 * @brief I2S3 Initialization Function
 * None
 * @retval None
 */
static void MX_I2S3_Init(void)
{

 /* USER CODE BEGIN I2S3_Init 0 */
 /* USER CODE END I2S3_Init 0 */

 /* USER CODE BEGIN I2S3_Init 1 */
 /* USER CODE END I2S3_Init 1 */
 hi2s3.Instance = SPI3;
 hi2s3.Init.Mode = I2S_MODE_MASTER_TX;
 hi2s3.Init.Standard = I2S_STANDARD_PHILIPS;
 hi2s3.Init.DataFormat = I2S_DATAFORMAT_16B;
 hi2s3.Init.MCLKOutput = I2S_MCLKOUTPUT_DISABLE;
 hi2s3.Init.AudioFreq = I2S_AUDIOFREQ_16K;
 hi2s3.Init.CPOL = I2S_CPOL_LOW;
 hi2s3.Init.ClockSource = I2S_CLOCK_PLL;
 hi2s3.Init.FullDuplexMode = I2S_FULLDUPLEXMODE_DISABLE;
 if (HAL_I2S_Init(&hi2s3) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN I2S3_Init 2 */
 /* USER CODE END I2S3_Init 2 */

}

/**
 * @brief GPIO Initialization Function
 * None
 * @retval None
 */
static void MX_GPIO_Init(void)
{
 GPIO_InitTypeDef GPIO_InitStruct = {0};
/* USER CODE BEGIN MX_GPIO_Init_1 */
/* USER CODE END MX_GPIO_Init_1 */

 /* GPIO Ports Clock Enable */
 __HAL_RCC_GPIOC_CLK_ENABLE();
 __HAL_RCC_GPIOH_CLK_ENABLE();
 __HAL_RCC_GPIOA_CLK_ENABLE();
 __HAL_RCC_GPIOB_CLK_ENABLE();

 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(LD2_GPIO_Port, LD2_Pin, GPIO_PIN_RESET);

 /*Configure GPIO pin : B1_Pin */
 GPIO_InitStruct.Pin = B1_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_IT_FALLING;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(B1_GPIO_Port, &GPIO_InitStruct);

 /*Configure GPIO pins : USART_TX_Pin USART_RX_Pin */
 GPIO_InitStruct.Pin = USART_TX_Pin|USART_RX_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 GPIO_InitStruct.Alternate = GPIO_AF7_USART2;
 HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

 /*Configure GPIO pin : LD2_Pin */
 GPIO_InitStruct.Pin = LD2_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(LD2_GPIO_Port, &GPIO_InitStruct);

/* USER CODE BEGIN MX_GPIO_Init_2 */
/* USER CODE END MX_GPIO_Init_2 */
}

 

 

 

 Any idea of what im doing wrong?

Thanks in advance

1 reply

KDJEM.1
Technical Moderator
September 20, 2024

Hello @GaelicThunder and welcome to the Community;

 

Could you please check the BSY bit when SPI is disabled?

Is it  stay high when SPI is disabled?

Please take a look at this errata precisely section SPI/I2S may help you.

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate
September 20, 2024

Hello KDJEM.1, thanks for the welcome!

I ended up being able to use both I2S using DMA, and the results seems ok.
I didn't check too much why it wasn't working before, since i had to work on another project.

I will check the errata you sent me and do some test about in on monday, just to be sure.
Thanks a lot!