Skip to main content
Visitor II
July 25, 2024
Solved

STM32F103C8 to connect st link v2

  • July 25, 2024
  • 1 reply
  • 1106 views

Hi,
I am using UP Xtreme edge compute i5 kit and trying to program the STM32F103C8 MCU which is available in the UP Xtreme kit via ST link V2. but i'm unable to find out the debugging pins like jtag/swd pins on STM32. can anyone please fix this problem
Thank you

Best answer by STTwo-32

Hello @Nageshk and welcome to the ST Community :smiling_face_with_smiling_eyes:.

If you arr looking for the JTAG/SWD Debug pins. You have just to look for the JNTRST pin is PB4, JTDI pin is PA15, JTDO pin is PB3, JTMS/SWDIO pin is PA13 and JTCK/SWCLK pin is PA14. They are available on the

Table 5. Medium-density STM32F103xx pin definitions of the DS5319.

Best Regards.

STTwo-32 

1 reply

STTwo-32
STTwo-32Best answer
Technical Moderator
July 25, 2024

Hello @Nageshk and welcome to the ST Community :smiling_face_with_smiling_eyes:.

If you arr looking for the JTAG/SWD Debug pins. You have just to look for the JNTRST pin is PB4, JTDI pin is PA15, JTDO pin is PB3, JTMS/SWDIO pin is PA13 and JTCK/SWCLK pin is PA14. They are available on the

Table 5. Medium-density STM32F103xx pin definitions of the DS5319.

Best Regards.

STTwo-32