STM32F103RB Nucleo – Debug fails after programming (“Target is not responding” in ST-LINK GDB Server)
Hello,
I am working with an STM32F103RB Nucleo board. I am able to successfully connect and program the device using ST-LINK, but I am facing an issue during debugging.
The code is downloaded successfully and verified, but when the debugger tries to run (after the 'cont' command), it fails with the following error:
Error in executing 'cont' command
Target is not responding
Failed to read all registers from target
Setup details:
- Board: NUCLEO-F103RB
- ST-LINK Firmware: V2J47M34
- STM32CubeProgrammer: v2.20.0
- Debug Interface: SWD
- Connection Mode: Under Reset
- Reset Mode: Hardware reset
- SWD Frequency: 125 kHz
Observations:
- Programming completes successfully
- Verification is successful
- Issue occurs only when starting execution/debugging
Things I would like help with:
1. What could cause the target to stop responding immediately after programming?
2. Could this be related to clock configuration or incorrect startup code?
3. Are there specific debug settings (reset mode, SWD frequency, etc.) I should modify?
ERROR: -
STMicroelectronics ST-LINK GDB server. Version 7.11.0
Copyright (c) 2025, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
-------------------------------------------------------------------
STM32CubeProgrammer v2.20.0
-------------------------------------------------------------------
Log output file: C:\Users\SRINAT~1.WOR\AppData\Local\Temp\STM32CubeProgrammer_a29124.log
ST-LINK SN : 066DFF495786534867176025
ST-LINK FW : V2J47M34
Board : NUCLEO-F103RB
Voltage : 3.27V
SWD freq : 125 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x410
Revision ID : Rev X
Device name : STM32F101/F102/F103 Medium-density
Flash size : 128 KBytes
Device type : MCU
Device CPU : Cortex-M3
BL Version : --
Opening and parsing file: ST-LINK_GDB_server_a29124.srec
Memory Programming ...
File : ST-LINK_GDB_server_a29124.srec
Size : 8.20 KB
Address : 0x08000000
Erasing memory corresponding to segment 0:
Erasing internal memory sectors [0 8]
Download in Progress:
File download complete
Time elapsed during download operation: 00:00:02.645
Verifying...
Time elapsed during verifying operation: 00:00:00.900
Download verified successfully
Error in executing 'cont' command ...
Target is not responding, retrying...
Failed to read all registers from target
Target is not responding, retrying...
Shutting down...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...