STM32F405RGT6 custom board connection issue with stm32cubeprogramer and stm32cubeIDE
Hello everyone.
I have recently made my own STM32 board based on the STM32F405. After soldering all the components and testing all pads and connections, finding them to be wired correctly and checking that the 3.3V is being supplied to all the correct pins, I tried to upload some code, but to my shock, the STM32F405 isn't establishing a connection via the ST-Link V2 nor the USB cable. After trying multiple fixes, I suspect the issue might be the STM32F405 chip that I got off AliExpress itself.
Before taking any further steps to replace it, I decided to post a question here for review in case the problem was in my PCB design. And sure enough, I had misplaced the chip pin due to the faulty pinout diagram I used as reference.
I have since fixed the chip's orientation and rechecked all pad and pin connections, as well as the 3.3V supply, and found everything to be correct; yet I still cannot get the STM32 CubeProgrammer or IDE to connect with my board using the ST-Link V2 or a USB Type-C.
If you have any remarks on what might have caused this problem, please share them.
NOTE: The -B label is referring to ground, and P is the VCC.
PROBLEM:

BOARD: