Skip to main content
Mr_flux
Associate
July 17, 2024
Solved

STM32F413ZH breakout board

  • July 17, 2024
  • 2 replies
  • 2369 views
  • Are there any STM32F413ZH breakout boards?

IMG_5628.jpeg

Best answer by Andrew Neil

The connectors are 0.1" pitch - so you can easily connect to standard prototyping boards.

The "Zio" connectors are compatible with the Arduino R3 shield pinout:

AndrewNeil_0-1721234510372.png

https://www.st.com/resource/en/user_manual/um1974-stm32-nucleo144-boards-mb1137-stmicroelectronics.pdf

 

So you could use any Arduino shield which provides suitable JST and/or terminal block connections

2 replies

Andrew Neil
Super User
July 17, 2024

you mean apart from the Nucleo-F413ZH ?

https://www.st.com/en/evaluation-tools/nucleo-f413zh.html

 

What, exactly, do you want from this "breakout board" that the Nucleo-F413ZH doesn't provide?

Does it have to be exactly an STM32F413ZH, or would other family members do? If so, give details.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Mr_flux
Mr_fluxAuthor
Associate
July 17, 2024

 

Thank you for your reply!

Yes, I am aware of the Nucleo-F413ZH board. However, I am looking for a breakout board that allows me to easily integrate JST connectors or terminal blocks for my specific application.

I would prefer to stick with the STM32F413ZH due to specific project requirements. However, if no such breakout board exists for this MCU and there are similar family members (like the STM32F41x series) with more suitable breakout boards, I would be open to considering those.

Andrew Neil
Andrew NeilBest answer
Super User
July 17, 2024

The connectors are 0.1" pitch - so you can easily connect to standard prototyping boards.

The "Zio" connectors are compatible with the Arduino R3 shield pinout:

AndrewNeil_0-1721234510372.png

https://www.st.com/resource/en/user_manual/um1974-stm32-nucleo144-boards-mb1137-stmicroelectronics.pdf

 

So you could use any Arduino shield which provides suitable JST and/or terminal block connections

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Tesla DeLorean
Guru
July 18, 2024

Amazon has JST connector and cable kits. 

You can solder wires into the thru-holes, or use shields as an intermediary, or make quick turn interposer boards via PCBWAY etc to solder connectors too.

If you have breakout connectors you could wirewrap those to pin headers as a more robust implementation than dupont wires.

Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..