Skip to main content
Associate
April 20, 2024
Question

STM32F427VIT6 flash mode

  • April 20, 2024
  • 2 replies
  • 1064 views

Hello,

 

I have a custom PCB with STM32F427VIT6. 

Been reading and learning a lot about MCU's in general. I'm very new to all of this so please bare with me.

When PCB is connected to the PC via usb, it shows up as HID device (it emulates gamepad/controller).

I'll assume it has a custom bootloader and firmware

 

The PCB comes with a custom .exe for flashing directly via USB. It also comes with a custom dump .exe

PCB comes with 1 USB-C (act as UART maybe?)

The custom .exe can be flashed via USB after I put it in DFU mode I presume? (I hold the boot button, it flashes a specific color to allow the flashing). I can click on flash, restore, or even backup basic configs. once I unplug, plug back in, it becomes operational. The way I put it in flash mode is by having the PCB off, keep ressing boot button then pluggin the USB.

I would like to retrieve the firmware/bootloader so I can test it in another board. I tried STM32Cube, ST flash, and many others, but it doesn't seem to recognize any connectivity.

Any help or guidance would be appreciate.

2 replies

Amel NASRI
Technical Moderator
June 25, 2024

Hi @fabrecordz ,

If you have already found an answer to your question, that would be great to update the Community.

Otherwise, you can use STM32CubeProgrammer to test with other boards using bin, hex, elf or srec file.

To use STM32CubeIDE, you need to have the source code for the project to be flashed available on your end.

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Visitor II
February 10, 2025

Hi @fabrecordz, have you figured out how to dump the bootloader on this device? I know exactly what device you are talking about.