Skip to main content
Associate
November 8, 2024
Question

STM32F446RE, SPI TX and Digilent ADP3450

  • November 8, 2024
  • 1 reply
  • 892 views

There's a ghost in the machine!  Look at waveforms; CS randomly goes high during HAL_TransmitReceive.

 

uint8_t		EMIT_REG_I
( uint8_t R_I )
{
 uint8_t Ret_D;

 CS_0;
 DC_0;

 // SPI.TX
 Ret_D		= SPIx_Write ( R_I );

 CS_1;

 return		Ret_D;
}




uint8_t		EMIT_REG_V
( uint8_t R_V )
{
 uint8_t	Ret_D;

 CS_0;
 DC_1;

 Ret_D		=	SPIx_Write	( R_V );

 CS_1;

 return		Ret_D;
}



uint8_t		EMIT_REG_X
( uint8_t R_I, uint8_t R_V )
{
 EMIT_REG_I		( R_I );
 EMIT_REG_V		( R_V );

 return		0;
}


// TX Register Index and Register Index-'s Value
EMIT_REG_X		( 0xEB, 0x20 );

 

 

OS: Linux Ubuntu, Noble Numbat

WaveForms (3.23.4) and Adept installed from .deb package

 

Using Digilent ADP3450 to Measure SPI Protocol Logic Levels on an STM32F446RE.

SPI Baudrate is 4 MHz.

 

Digital GND on the ADP3450 is connected to GND on the STM32F446RE

DIO_0 is connected to SPI.CS on the STM32

DIO_1 is connected to SPI.SCK on the STM32

DIO_2 is conntected to SPI.MOSI on the STM32

DIO_3 is connected to SPI.MISO on the STM32

 

 

Using STM32 API HAL_SPI_TransmitReceive to TX Register Index and Register Value:

On Emit_X( 0xEB, 0x20 ) the logic waveform shows the following:

0xEB split apart, CS mysteriously goes high twice during TX

0x20 split apart, CS mysteriously goes high once during TX

 

What is the recommended fix?

1 reply

AtticusAuthor
Associate
November 10, 2024

Solved.

Spurious spikes on CS and DNC lines were caused by CrossTalk; forward and backward!