Skip to main content
Associate III
July 28, 2025
Question

STM32F469i-Disco Connecting different screens.

  • July 28, 2025
  • 1 reply
  • 196 views

Hello, 

I wanted to use these screen from aliexpress : 

Xenon02_0-1753741571203.png

It uses MIPI DSI and Touch Screen. 

Xenon02_1-1753741761063.png

I have no idea yet if touch pins are doubled on both sides. But I don't know how to connect these pins in the devboard which looks like that on the back ... 

Xenon02_3-1753741828752.png


Any suggestion how should I interpret these pinouts and how to connect on this board ? I am a bit new to this MIPI standard stuff. 

 

1 reply

QSHAO.1
ST Employee
July 29, 2025

Your LCD seems not pin to pin compatible with LCD connector CN10 and TP connector CN2 on 32F469IDISCOVERY, it may not be supported directly.  You may refer to 32F469IDISCOVERY schematic at https://www.st.com/resource/en/schematic_pack/mb1189-c01_schematic.pdf. thanks!

Xenon02Author
Associate III
July 29, 2025

I thought MIPI DSI is a standard that is has 30 pins. 
Which I guess in this screen touch pins are both in 7 pin connector and 30 pin connector which is weird ? I guess.

But nonetheless I thought MIPI DSI is a fixed standard which has predefined number of pins.