Skip to main content
Ajadh.1
Associate III
November 28, 2025
Question

Stm32G0 Nucleo is detecting as Jlink But want it to detect as stm stlink port

  • November 28, 2025
  • 3 replies
  • 1026 views

Hi,

I need some solution. Issue is stm32G0b1re nucleo board is detecting as Jlink device in device manager. But I want this to detect as STM stlink device. 

I have uninstall driver then it is decting as USB port. Even I have tried to install stsw-link009 driver. But somehow it is not installing driver. As I can't that in control manager. 

let me know what to be done to update driver so that I could see it as STM stlink device.

 

Thank You

3 replies

Technical Moderator
November 28, 2025

Hello @Ajadh.1 

Is it a genuine ST-Link? Refer to the following article to check if you are using a genuine ST-LINK/V2 or a cloned one: How to recognize a genuine ST-LINK/V2 versus a cloned one.

Make sure to install USB driver correctly.

Verify that the USB VBUS pin is properly powered and check that jumpers on the STM32G0 board are correctly connected. 

Check the tips on How to solve connection errors when connecting and programming the STM32 target board

"When your question is answered, please close this topic by clicking ""Accept as Solution"".ThanksImen"
Ozone
Principal
November 28, 2025

Why not using it as JLink, these debug adapters have wider toolchain support than ST-Links.

Segger has ST-Link firmware available on their website for free download, which allows one to convert onboard ST-Links into JLinks. The website also has a (Windows) tool to flash it.

Probably <somebody> converted this Nucleo board that way.

Download and install the tool, it also allows you to convert it back to ST-Link.

Andrew Neil
Super User
December 5, 2025

@Ajadh.1 wrote:

stm32G0b1re nucleo board is detecting as Jlink device in device manager.


And you are using the built-in debugger on the Nucleo board itself - via CN2 - yes?

AndrewNeil_0-1764931387245.png

 

In that case, you (or somebody before you) must have converted that ST-Link to a J-Link using Segger's converter:

https://www.segger.com/products/debug-probes/j-link/models/other-j-links/st-link-on-board/

 

You can use that same converter to reverse the process: Restore ST-Link Firmware.

 

 

PS:

If you have trouble with Segger's utility, you need to contact Segger for support - it's nothing to do with ST:

https://www.segger.com/support/technical-support/

https://forum.segger.com/board/4-j-link-flasher-related/

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.