Skip to main content
Associate II
June 21, 2024
Question

STM32G031K8 Nucleo Error in RAM

  • June 21, 2024
  • 2 replies
  • 879 views

Hi

We've got here 3 STM32G031K8 Nucleo. 2 of them had problems with RAM access. 1 works fine at the moment.

For example STM32CubeProgrammer shows by RAM Dump

Prog.png

Keil shows 

keil.png

STLink Utilities hangs by Access of some RAM address.

 

Is this a known Problem?

Is there a workaround?

Can you replace the faulty Nucleo?

 

 

2 replies

Technical Moderator
June 21, 2024

Hello @CanRF ,

You can try to read option bytes with STM32CubeProgrammer.

Verify at Option Bytes if Read Out Protection is unchecked.

"When your question is answered, please close this topic by clicking ""Accept as Solution"".ThanksImen"
CanRFAuthor
Associate II
June 22, 2024

I can readout the flash without an problem.

I can readout most part of the RAM.

But on some address I get this error (STM32CubeProgrammer) or '?' (Keil)

I think the chip has a bad RAM.