Skip to main content
jean
Senior
July 21, 2022
Question

STM32H7 very hot

  • July 21, 2022
  • 12 replies
  • 8556 views

Hello dear community,

I've started using STM32H743VGT6 on a custom board I've made.

I'm testing the hardware now and I quickly detected that the temperature is really high (approx. 70°c on the top of the chip package).

I have another board, based on a STM32H743BIT6, quite similar, and the temperature of this one seems normal (approx. 40°C)

  • dividing the H7 clock speed by 2 really helps to reduce the temperature, but my original clock config seems right (tested with cubeMX)
  • It's not easy for me to measure the current drawn by the H7, as the 3V3 is used by many other devices

Have you ever experienced that kind of issue?

Thanks a lot, have a nice day!

Jean

12 replies

Associate
June 27, 2024

Thank you this topic i have design my board with stm32H723  i need maximum adc speed  so set clock to 550 Mhz but the chip is hot . i have down to 400 Mhz   founded temperature cool down . but adc sample rate down too. why?

 

Tesla DeLorean
Guru
June 27, 2024

Synchronous?

Check clock sources and dividers servicing the ADC.

Here we tend to unpack the RCC settings to confirm we understand the Reference Manual and what we ended up with.

Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..
KNaim.1
Associate III
August 5, 2024

Thank a lot for this post because i have made my pcb too base on stm32h750 the mcu is very hot  at 480mhz i am going to try to reduce speed to see if any changes..  i was thinking about my design because i have put all the capacitors like intel processor on bottom layer pcb to have them close has possible from their respetive pin.

The power supply is ams1117 and its working good that deliver 3.29 volt dc and its not hot.

 

 

Tesla DeLorean
Guru
August 5, 2024

What kind of hot? Uncomfortable or burns to your finger hot?

The latter indicates something seriously wrong, and a conduction path you don't want. ie Internal LDO outputting 1.25V into 3.3V supply rails.

The AMS1117 can push an AMP. Might suggest you check how much your circuit is drawing vs reasonable expectations.

Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..
KNaim.1
Associate III
August 6, 2024

Thanks DeLorean

Here is my pcb design stm32h750 pcb.pngstm32h750_pcb back.pngpcb_stm32h750.png

 

It's my first stm32 pcb sure that it's not perfect because i am learning i am comming from esp32 world that is really more simple. 
I have faced some problems with clock ic  at the begining   because i have buy by mistake 3 states clock(with no data sheet Aliexpress is not perfect.but it's affordable..) and not crystal. (but achieve to make it work).
- QSPI and Spi flash are working perfect i have follow Controltech tuto on youtube  and all result was good.

- what value of resistor do you recommand for input pullup on stm32h750 pins ?