Skip to main content
Associate
July 24, 2024
Question

STM32H735IGT6 equivalent Nucleo Board

  • July 24, 2024
  • 3 replies
  • 1785 views

Which NUCLEO board is suitable for STM32H735IGT6 microcontroller.

3 replies

STTwo-32
Technical Moderator
July 24, 2024

Hello @durgamaravind1077 and welcome to the ST Community :smiling_face_with_smiling_eyes:.

There is no Boards (Nucleo, DK or Eval) that use the STM32H735IGT6. The only board that embeds an STM32H735 is the STM32H735G-DK (Based on the STM32H735IGK6 MCU).

Best Regards.

STTwo-32

Associate
July 24, 2024

which nucleo board is suitable.

STTwo-32
Technical Moderator
July 24, 2024

As I've already said, "There is not a Nucleo board based on this MCU". The Nucleo boards are evaluation boards that are available only for a few MCUs and not all of them.

Best Regards.

STTwo-32

Andrew Neil
Super User
July 24, 2024

@durgamaravind1077 wrote:

Which NUCLEO board is suitable for STM32H735IGT6 microcontroller.


As always, go to the Product Page for that chip, on the 'Tools & Software' tab look for 'Evaluation Tools':

AndrewNeil_0-1721813973630.png

https://www.st.com/en/microcontrollers-microprocessors/stm32h735ig.html#tools-software 

 

Follow the link:

AndrewNeil_1-1721814092465.png

 

As @STTwo-32 said, the only option is the STM32H735G-DK:

https://www.st.com/en/evaluation-tools/stm32h735g-dk.html

 

 

 

 

 

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
LCE
Principal II
July 24, 2024

Nucleo-H723 is the closest to the H735.

Except for some missing peripherals, these MCUs are 100% compatible.

But don't forget: the Nucleo-board has almost no extra stuff equipped: no external RAM, no flash, no... other stuff.