Skip to main content
Explorer II
February 10, 2025
Solved

STM32H747I-DISCO built-in display issue

  • February 10, 2025
  • 2 replies
  • 576 views

I am working on a project using the built-in LCD display of the STM32H747I-DISCO board. However, the display output shows unintended thin lines and color distortions, appearing as if the colors are breaking. I am unsure whether this issue is caused by a hardware defect in the display itself or a misconfiguration in the IOC settings and debugging process.

 

To troubleshoot, I ran the TouchGFX game example without any modifications, but the same issue persists. I would appreciate any insights or suggestions on how to resolve this.....

 

IMG_8433C6A6F16A-1.jpegIMG_5854.jpeg

Best answer by mƎALLEm

Hello @junseok3607 ,

As said by @AScha.3 it could be a HW issue. Try to upload the board Demo from here and check if you have the same lines at the same positions. If you don't have a such issue with the demo, it's a software issue.

 

2 replies

AScha.3
Super User
February 10, 2025

If the not working line is on constant position, if running different software/programs, it probably a hardware problem.

The TFT protective foil shows, it had already experienced a lot of treatment/use...

So pressing a little on the outer TFT area /contact/connectors -  are any changes on the display errors?

(most times this is a lost/bad contact to a line )

"If you feel a post has answered your question, please click ""Accept as Solution""."
mƎALLEm
mƎALLEmBest answer
Technical Moderator
February 10, 2025

Hello @junseok3607 ,

As said by @AScha.3 it could be a HW issue. Try to upload the board Demo from here and check if you have the same lines at the same positions. If you don't have a such issue with the demo, it's a software issue.

 

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question."