Question
STM32H753-EVAL -- Use DB9 port (CN2) as usart 1
- April 27, 2026
- 1 reply
- 108 views
Hie, according to the documentation of the board, USART1 can be used with db9 port by setting up JP7 and JP8 to 1 and 2 ( which I did). The second thing is to connect usart_tx and usart_rx to PB14 and PB15.
The problem is that nothing is showing up on the pc with DB3 port. I've check the tx port with an oscilloscope and I'm getting signal on data sending but only 1.1 V (in AC). I don't know if it's part of the issue but I hope someone has the solution
Thanks