Skip to main content
Associate III
June 6, 2024
Solved

STM32H755 QSPI Compatibility - Infineon S25FL128SAGNFM003

  • June 6, 2024
  • 3 replies
  • 1120 views

Hello community,

I wanted to know how can I check the compatibility of of QSPI NOR FLASH with micro-controller, what are the parameter that will affect selection.

Are Infineon chips supported by STM32H7 family especially S25FL128SAGNFM003.

Best answer by Tesla DeLorean

The Hardware supports the part.

The Software must suitably configure the part and walk it into the correct/desired mode of operation at both ends.

Timing, must meet those specified by the chip, and the performance of the traces / pin drivers.

Choice of commands, bit lengths / widths of the phases, sufficient "dummy" cycles for the part to prefetch a buffer/line of data, or a couple, so it can stream bytes at high speeds, independently of the speed to fetch from the array.

A 16MB (128Mb) device can be addressed via 24-byte (3-byte) address, large devices will need 4-bytes, that mode may either need to be selected, or different sub-set of commands used.

You will be expected to read the data sheets and manuals for both the memory IC, and the MCU, to fully understand the expectations on both ends.

 

To program content, tools like STM32 Cube Programmer, need an "External Loader" that is aware of your part choice, board clocks, and board wiring. Given the wide variety of pin combinations these need to be customized to circumstances.

The Erase is a bit complicated, as there's a mix of sector sizes at the front/back (4KB), rest (64KB)

Got some support for the 256Mb models, and could likely add support for the 128Mb ones.  https://github.com/cturvey/stm32extldr/tree/main/h7_s25sl256

3 replies

KDJEM.1
Technical Moderator
June 6, 2024

Hello @sarun ,

 

To check whether a device is supported by QUADSPI interfaces, it is recommended to refer to the device datasheet and to the RM0434 15 Quad-SPI interface (QUADSPI) section and check if the command format and order in the datasheet memory are in line with the QUADSPI frame format and order (Instruction, Address, Alternate, Dummy, Data).

Each command can include five phases: instruction, address, alternate byte, dummy, data. Any of these phases
can be configured to be skipped, but at least one of the instruction, address, alternate byte, or data phase must be present.

KDJEM1_0-1717670003530.png

 

Also the AN4760 Application note section 8 Supported devices, can also help you check memory compatibility with the QUADSPI interface.

KDJEM1_1-1717670621093.png

Thank you

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Tesla DeLorean
Tesla DeLoreanBest answer
Guru
June 6, 2024

The Hardware supports the part.

The Software must suitably configure the part and walk it into the correct/desired mode of operation at both ends.

Timing, must meet those specified by the chip, and the performance of the traces / pin drivers.

Choice of commands, bit lengths / widths of the phases, sufficient "dummy" cycles for the part to prefetch a buffer/line of data, or a couple, so it can stream bytes at high speeds, independently of the speed to fetch from the array.

A 16MB (128Mb) device can be addressed via 24-byte (3-byte) address, large devices will need 4-bytes, that mode may either need to be selected, or different sub-set of commands used.

You will be expected to read the data sheets and manuals for both the memory IC, and the MCU, to fully understand the expectations on both ends.

 

To program content, tools like STM32 Cube Programmer, need an "External Loader" that is aware of your part choice, board clocks, and board wiring. Given the wide variety of pin combinations these need to be customized to circumstances.

The Erase is a bit complicated, as there's a mix of sector sizes at the front/back (4KB), rest (64KB)

Got some support for the 256Mb models, and could likely add support for the 128Mb ones.  https://github.com/cturvey/stm32extldr/tree/main/h7_s25sl256

Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..
sarunAuthor
Associate III
June 7, 2024

Thank you for your inputs now I have a clear picture, did digging through data sheet of the component i needed and the components mentioned in AN4760, other than the alternate byte phase everything looks fine. yes as @KDJEM.1 mentioned it can be configured to skip and it is mentioned in section 3.1.3 of the the AN4760. 

Once again Thank you for your input @Tesla DeLorean  and @KDJEM.1