Skip to main content
Visitor II
March 17, 2025
Question

STM32H755BIT3 Supply connection

  • March 17, 2025
  • 1 reply
  • 499 views

你好

我正在与 STM32H755BIT3 一起做项目。
我设计的电路板的现状是,用DC-DC 3.3V电源上电后,芯片很快发热严重,不出现短路就无法下载程序。我推测这是由于外围电路的设计。

有人可以帮忙找出问题所在吗?

提前感谢大家的任何提示。

Translation:

Hello

I am working on a project with the STM32H755BIT3.
The current situation of the board I designed is that after powering up with a DC-DC 3.3V power supply, the chip quickly heats up severely and the program cannot be downloaded without a short circuit. I have a doubt about the hardware.

Can anyone help to find out what the problem is?

Thank you all in advance for any tips.

1 reply

AlexWEI
ST Employee
August 14, 2025

the sch is too difficult to read for it, did you solved the issue?